The LioN Management Suite – LMS is a free of charge stand alone software application.
With its ease of use it provides time and cost saving for automation engineers by
- Discover all LioN-Power IO modules in a Local Area Network (LAN)
- Perform firmware upgrades across multiple device in parallel
FAQs
- Can LioN-Power devices be detected via routers?
- No, detection of LioN-Power devices is only possible within a LAN.
- How many devices can be updated simultaneously?
- The action can be started on all discovered devices at the same time.
- Depending on the PC performance the execution of the update might be partly consecutive.
- Which operating system are support?
- The LMS was tested with Windows 7 and Windows 10.